AXIS#.IL.FB
Description
This parameter displays the measured actual q-component current reading.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Arms |
Range |
± Axis peak current (AXIS#.IPEAK ) |
Default Value |
N/A |
Data Type |
Float |
See Also |
N/A |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AXIS1.IL "Instruction List" This is a low-level language and resembles assembly.FB |
500ah |
01h |
Signed32 |
- |
1000:1 |
Read only |
Yes |
AXIS2.IL.FB |
510ah |
01h |
Signed32 |
- |
1000:1 |
Read only |
Yes |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.IL.FB |
5803 |
16AB |
Signed32 |
Read Only |
- |
AXIS2.IL.FB |
71339 |
116A |
Signed32 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.IL.FB |
5803 |
Float |
Read Only |
- |